Cannot debug MCXN947

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Cannot debug MCXN947

1,728 Views
TomC818
Contributor III

Hello, I have a customized MCXN947 board which both the internal LDO and DCDC have been bypassed. Now I am trying to program the board with Segger JLINK. Using the JLink Commander the host computer can detect and identify the M33 core.

TomC818_1-1752216222533.png

 

But when I tried to flash any thing to the mcu, the host computer cannot identify the target device.

TomC818_2-1752216397028.png

My board currently have used PCA9420 to provide the power to the VDD_CORE and IOs. I have followed the datasheet and pull the VDD_DCDC low with 10k resistor and left DCDC_LX floated. The VDD_LDO_CORE pin is also shorted to the VDD_CORE.


I have tried both vscode and mcxpressor which both have failed to flash the codes onto the chip. But yet the JLINK can identify the processor core. 

Labels (3)
0 Kudos
Reply
1 Reply

1,681 Views
Celeste_Liu
NXP Employee
NXP Employee

Hello @TomC818 ,

Thanks for your post.

I tried using J-Link with the FRDM-MCXN947 board, and there were no issues.

Please refer to our UG10092 and the FRDM board schematic to check your hardware design, with a focus on the power supply and SWD interface.

UG10092: https://www.nxp.com/webapp/Download?colCode=UG10092&location=null&isHTMLorPDF=HTML

Hope it can help you.

BRs,

Celeste

 

-----------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!
-----------------------------------------------------------------------------------------------------------------

0 Kudos
Reply