MQTT with TLS on MCXN947

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MQTT with TLS on MCXN947

691 Views
nxpsachve
Contributor I

Hi,

    Is it possible to have security(wolfssl or mbedtls) with MQTT on MCXN947. I'm using FRDM board and couldn't find any combination of mqtt with tls or ssl examples. Is there any way to integrate security with MQTT on MCXN947?

Regards,

Sach

Labels (1)
0 Kudos
Reply
3 Replies

646 Views
Harry_Zhang
NXP Employee
NXP Employee

Hi @nxpsachve 

Yes, currently, there is no related demo about combination of mqtt and tls.

BR

Harry

0 Kudos
Reply

638 Views
nxpsachve
Contributor I
Hi Harry,
Do you have any suggestions for achieving this on the MCXN947, such as using a particular repository or resource that can be adapted for the board?
Regards,
Sach
0 Kudos
Reply

569 Views
Harry_Zhang
NXP Employee
NXP Employee

Hi @nxpsachve 

I suggest that you can 

start with mbedTLS + MQTT because:

Both are in the SDK

Easier integration path

Supported by many embedded projects.

BR

Harry

0 Kudos
Reply