Assistance Needed: Datasheet and BDM Pinout for SC505407VFC Microcontroller (D151851-4410)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Assistance Needed: Datasheet and BDM Pinout for SC505407VFC Microcontroller (D151851-4410)

3,522件の閲覧回数
Hemand444
Contributor I

Hello everyone,

I’m trying to find the datasheet or BDM pinout for the microcontroller on this ECU board (photo attached). The microcontroller details are:

IMG_0567.jpg

 

D151851-4410

SC505407VFC

-180

QQFW02490

 

If anyone has information or can help identify the BDM points, I’d really appreciate it. Thanks in advance!

ラベル(1)
0 件の賞賛
返信
5 返答(返信)

3,459件の閲覧回数
Hemand444
Contributor I

If we look at similar structures, the section I marked in the red box might be the BDM interface of my ECU. However, I can see 12 pins, while BDM interfaces typically have a maximum of 10 pins. Is there any possibility that this could still be a BDM interface with 12 pins?

0 件の賞賛
返信

3,461件の閲覧回数
Hemand444
Contributor I

I found this image in another forum where they mention that the 8 pin section in the top right(marked in yellow box) is the BDM interface. The microcontroller in this image has a similar part number to mine, so I believe they might share the same architecture.

0 件の賞賛
返信

3,484件の閲覧回数
Celeste_Liu
NXP Employee
NXP Employee

Hello @Hemand444 ,

Thanks for your post.

I haven't found any information related to SC505407VFC on our official website. Sorry for any inconvenience caused. Are you sure it is from NXP? Would you please tell me your purchasing channel so that I can confirm it more accurately? 

BRs,

Celeste

 

 

0 件の賞賛
返信

3,468件の閲覧回数
Hemand444
Contributor I

Hi Celeste,

Thanks for your response. I understand that SC505407VFC is not listed on the official NXP website. However, I found a similar microcontroller labeled D151851-0860/SC416887VFC/185/QSGX9921C, which appears to be a variant of the Motorola/Freescale MC68H16 R series 

Given this similarity, could you confirm whether SC505407VFC belongs to the same family or if it shares a similar architecture? Any information on the datasheet, pinout, or potential BDM access points would be greatly appreciated.

Looking forward to your insights.

0 件の賞賛
返信

3,368件の閲覧回数
Celeste_Liu
NXP Employee
NXP Employee

Hello @Hemand444 ,

Please refer to AN2387.fm. There is content related to BDM in it.

BRs,

Celeste

0 件の賞賛
返信