Hi, all
Just started to learn zephyr project with VS code, import a few examples like hello_world and button, they work fine , but I noticed they all use external RAM like below:
Hello, Diego
Thanks for reply.
Yes, I am using RT1024. I would like to move whole application into Zephyr, so it has RTOS, currently it is bare metal. I reconfigured FlexRAM according to the application note and it works fine. And in production already.
Just thinking of the way forward and new to Zephyr RTOS, is there an easy way to migrate?
Regards!
Ping
 diego_charles
		
			diego_charles
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hi @ping1
I am glad to know that our application note helped you!
Regarding Zephyr, drivers change a bit and you are now operating with a device tree. There is a training made by my colleague Dereck that may help you Application Portability Made Easy With Zephyr™ OS and NXP
Regards,
Diego
Hi, Diego
It helped me when I develop bare metal application use MCUXpress, but it seems not apply to Zephyr project. I went thought the video too, it is a good one, and covers basic things well, But I am still nor sure how to reconfigure RAM after that, hence asking for help here.
Thank you!
Ping
 diego_charles
		
			diego_charles
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hi @ping1
My apologies for not getting back to you sooner.
Considering that you have development with Zephyr RTOs, I have to mention that we encourage Zephyr RTOs users to use the Zephyr GitHub. As stated in https://community.nxp.com/t5/Zephyr-Project/bd-p/Zephyr-Project.
In the Zephyr github, there is a thread that I hope is still of interest or help Run entire application from RAM #36800 This post details how to execute from internal SRAM, in this case, ITCM, first by changing the CODE_LOCATION to this memory
All the best,
Diego
 diego_charles
		
			diego_charles
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hi @ping1
I hope that you are doing well!
It looks like you are using an i.MX RT10xx, could you please specify?
Would you like to move whole application or some secitons of code or variables?
If you need to reconfigure FlexRAM you can check this application note: AN12077: Using the i.MX RT FlexRAM – Application Note This app note goes into details of possible re-arragements of the flexRAM. Please keep in mind that for development and evaluation purposes you will need to modify some fleRAM registers to change flexRAM arragement , but for production, is advisable to burn fuses.
Best regards,
Diego