Using config tools with vscode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Using config tools with vscode

ソリューションへジャンプ
4,345件の閲覧回数
mttjcksn
Contributor II

Hi there, 

I'm getting started with the RT1170EVK and want to use vscode for development.

I'm following all the tutorials here: https://github.com/nxp-mcuxpresso/vscode-for-mcux/wiki/Working-with-MCUXpresso-SDK
However, I'm currently stuck on missing drivers.

Here's my workflow:


- 'Installed' SDK repository with MCUXpresso extension in vscode

- Import blinky example for my EVK

- Right-click project in vscode 'projects' view and check the respository and toolchain are associated correctly under 'configure. 

- Right-click project in vscode 'projects' view and check all components I need have been selected under 'configure'.

- Check the project builds and runs ok

- Right-click project in vscode 'projects' view and go to 'configure > Open with MCUXpressor Config Tools'


Now, when I add peripherals, it complains that the drivers cannot be found:

mttjcksn_0-1708539259038.png

How do I get it to find these drivers?
I have managed to get the project to compile by manually editing the cmake files, but it is cumbersome and the config tool still shows lots of errors.

I'm also struggling to find any examples that use this generated code from the config tool. All the examples seem to use the fsl drivers directly and so do not help in learning the API very much.

Many thanks, Matt.

0 件の賞賛
返信
1 解決策
4,300件の閲覧回数
Alex_Wang
NXP Employee
NXP Employee

Hi, @mttjcksn 

        According to your description, the tool doesn't recognize it. I tried to reproduce it, and my project code can be generated normally, we just need to change the generated code directory.

       I used MCUXpresso Config Tools v15, and I recommend you try again with the latest version. When we open MCUXpresso Config Tools through VS Code, click "Configure Preferences" under "Edit" in the toolbar, and the reference window is as follows:

Alex_Wang_0-1708918241484.png

       Click Edit to enter the window, add new rules as follows:

Alex_Wang_1-1708918389557.png

      Once this is done, you can generate the code into the vs code project.

      Hope this helps you.

Best regards, Alex

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
4,301件の閲覧回数
Alex_Wang
NXP Employee
NXP Employee

Hi, @mttjcksn 

        According to your description, the tool doesn't recognize it. I tried to reproduce it, and my project code can be generated normally, we just need to change the generated code directory.

       I used MCUXpresso Config Tools v15, and I recommend you try again with the latest version. When we open MCUXpresso Config Tools through VS Code, click "Configure Preferences" under "Edit" in the toolbar, and the reference window is as follows:

Alex_Wang_0-1708918241484.png

       Click Edit to enter the window, add new rules as follows:

Alex_Wang_1-1708918389557.png

      Once this is done, you can generate the code into the vs code project.

      Hope this helps you.

Best regards, Alex

0 件の賞賛
返信
4,277件の閲覧回数
mttjcksn
Contributor II

I followed your instructions and the errors are no longer there, thankyou