This is my first foray into NXP chips, so there likely is some ridiculously obvious way to accomplish this--but I have yet to find it...
I've designed a PCB around an LPC5506 MCU: https://www.nxp.com/part/LPC5506JHI48
Time to write code. So I downloaded the VSCode MCUXpresso extension, and after downloading addons, toolchains, etc. via the MCUXpresso Installer, I have the complete MCUXpresso Repository version 24.x "main" downloaded, and can successfully compile an example "LED Blinky" for the LPC55S06. (Yes, LPC55S06, not the LPC5506.)
However, when creating a new project against the MCUXpresso SDK version 24.x, MCUXpresso will only allow me to select EVK/EVM boards. The closest option that MCUXpresso allows me to choose is the LPC55S06--and no, I can't type in LPC5506: the "Create Project" button is disabled unless I click on an existing EVK option...which is only the LPC55S06 or 55S69:
ddusty21_1-1753383206804.png
I don't think this is close enough to allow me to program an LPC5506, as it is quite different from the LPC55S06.
The only hint I've yet been able to find is in this thread where an LPC5506 is apparently successfully being leveraged: https://community.nxp.com/t5/MCUXpresso-Config-Tools/LPC5506-platform-drivers-power-error/m-p/123992...
where I notice that the SDK is "SDK_2.x_LPCXpresso5506 version 2.8.2", instead of the "SDK _24.x" version I downloaded. (Likely also is not the VSCode extension.)
But this doesn't make sense, as folders for the LPC5506 (and all the other variants) are scattered all throughout the entire SDK 24.x version I already downloaded:
ddusty21_0-1753382107860.png
Digging around, I found that I could download a "Remote Archive" specifically for the LPC5506:
ddusty21_3-1753384915392.png
And then I could "Import Example from Repository", and select the LPC5506-specific repository I'd downloaded.
But once again, I was forced to select the LPC55S06 development board:
ddusty21_4-1753385044025.png
And the resulting project configuration clearly shows the CPU specification as LPC55S06, not the LPC5506 I had specifically targeted with the repository:
ddusty21_5-1753385102470.png
So my question is this: HOW do I create an empty (or even "Hello World") project specifically targeting the LPC5506 with the VSCode MCUXpresso setup?
Or is the VSCode MCUXpresso extension simply not ready for real life use?