Example code performace different between VSCode and MCUExpresso IDE

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Example code performace different between VSCode and MCUExpresso IDE

2,800 次查看
Peter19
Contributor II

Using same example for FRDM-MCXN947 I get different output from benchmark unit test.

I assume that there are different compiler settings somewhere...

MCUXpresso FFT SDK Example (serial port)
==========================
CMSIS DSP benchmark fft test start.
arm_rfft_q15Test: 4 ms
arm_rfft_q31Test: 4 ms
arm_cfft_q15Test: 4 ms
arm_cfft_q31Test: 6 ms
arm_ifft_q15Test: 5 ms
arm_ifft_q31Test: 4 ms
arm_dct4_q15Test: 20 ms
arm_dct4_q31Test: 20 ms

CMSIS DSP benchmark fft test succeeded.


vscode FFT SDK Example (serial port)
======================
CMSIS DSP benchmark fft test start.
arm_rfft_q15Test: 4 ms
arm_rfft_q31Test: 4 ms
arm_cfft_q15Test: 5 ms
arm_cfft_q31Test: 4 ms
arm_ifft_q15Test: 5 ms
arm_ifft_q31Test: 4 ms
arm_dct4_q15Test: 44 ms
arm_dct4_q31Test: 39 ms

CMSIS DSP benchmark fft test succeeded.

 

0 项奖励
回复
4 回复数

2,766 次查看
Celeste_Liu
NXP Employee
NXP Employee

Hello @Peter19 ,

Thank you for posting the question in the community. I did the same test and indeed found the issue you described. Please allow me more time to analyze it. If there is an update, I will let you know in time.

BR,

Celeste

0 项奖励
回复

2,758 次查看
Peter19
Contributor II

Hi

My intent was to highlight that NXP might want to make sure that choice of IDE does not affect performance on target. Both IDE's uses same toolchain and libraries and versions thereof. I would say that even the executable should be binary identical.

I am not expecting any solution for me, I am expecting NXP to shape up validation.

0 项奖励
回复

2,609 次查看
Celeste_Liu
NXP Employee
NXP Employee

Hello Peter,

I conveyed your feedback to the IDE team. They expressed that they were glad to receive your feedback and gave the following views:

Strictly speaking, the different results between the two IDEs are unintended and hard to avoid. This is due to different build systems, potential differences between build flags used in manifest-based SDK packages and ARM GCC packages (e.g., optimization levels), different C libraries (redlib, newlib, newlib-nano), and so on. Most of the build process is controlled through the SDK manifest in the MCUXpresso IDE and CMake files in the MCUXpresso VS Code extension.

If you have any further questions or concerns, please feel free to let us know. We are always here to assist you.

Have a great day,

Celeste

0 项奖励
回复

2,744 次查看
Celeste_Liu
NXP Employee
NXP Employee

Hello @Peter19 ,

Thank you for your feedback. I appreciate you taking the time to share it. I will spend more time exploring this issue.

BR,

Celeste

0 项奖励
回复