Debugging app deployed to nor flash

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Debugging app deployed to nor flash

跳至解决方案
2,154 次查看
arunkumar_g
Contributor IV

Hello 

 

I'm using 1189EVK and loaded freertos hello world cm33 app to vscode. 

I want to build, deploy and debug that app. But when deploying vscode shows an error 

"Error: ENOENT: no such file or directory, open 'C:\NXP\MCUX_Provi_v9\bin\deviceInfo.json'" and indeed that file is not in that directory (provisioning tool version is 9.0.1). Is that vscode doen't support debugging on flash?

 

Thanks

 

0 项奖励
回复
1 解答
2,119 次查看
Melania
NXP Employee
NXP Employee

Hi,

Indeed you can have this problem if no rights, the issue is logged and will be addressed soon. In the mean time, please find attached the deviceInfo file. Remove the txt extension, copy it in the location and let me know if the problem is fixed.

Regards,

Melania.

在原帖中查看解决方案

0 项奖励
回复
1 回复
2,120 次查看
Melania
NXP Employee
NXP Employee

Hi,

Indeed you can have this problem if no rights, the issue is logged and will be addressed soon. In the mean time, please find attached the deviceInfo file. Remove the txt extension, copy it in the location and let me know if the problem is fixed.

Regards,

Melania.

0 项奖励
回复