SPT GUI not loading after terminal window

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

SPT GUI not loading after terminal window

跳至解决方案
5,026 次查看
nxf64834
NXP Employee
NXP Employee

Hi,

One of our customer has installed SPT v3 on Windows 10, 64 bit, 16GB RAM system . On double clicking the icon on desktop, terminal window comes(refer attached "image") and then disappears. SPT GUI screen is not getting loaded.

How to rectify this issue? 

Please let me know if any other information required.

Thanks!! 

0 项奖励
回复
1 解答
5,018 次查看
liborukropec
NXP Employee
NXP Employee

Hi Boby,

see previous post - https://community.nxp.com/t5/MCUXpresso-Secure-Provisioning/Secure-provisioning-tool-fails-at-startu...- what Region language do you have? Also you can execute it in the command line with "-v" argument, so the prompt window is not closed and error output should not be lost .

liborukropec_0-1626797164105.png

 

Regards,

Libor

在原帖中查看解决方案

0 项奖励
回复
2 回复数
5,019 次查看
liborukropec
NXP Employee
NXP Employee

Hi Boby,

see previous post - https://community.nxp.com/t5/MCUXpresso-Secure-Provisioning/Secure-provisioning-tool-fails-at-startu...- what Region language do you have? Also you can execute it in the command line with "-v" argument, so the prompt window is not closed and error output should not be lost .

liborukropec_0-1626797164105.png

 

Regards,

Libor

0 项奖励
回复
4,996 次查看
marek-trmac
NXP Employee
NXP Employee

Hi Boby,

we have reproduced the issue with unsupported Region settings and the thread was updated with latest info how to workaround the problem. Here is copy of updated info:

> I have reproduced the issue today. It seems SPT does not start if regional format is not listed in https://docs.wxwidgets.org/3.1.4/language_8h.html

> Workaround: select format from the list of supported languages.

> We're sorry for inconvenience.

Regards

Marek

Regards,
Marek


NOTE: If you find the answer useful, kindly click on [ACCEPT AS SOLUTION] button
0 项奖励
回复