CMSIS DAP FW v3 ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CMSIS DAP FW v3 ?

Jump to solution
4,022 Views
IvoBCD
Contributor III

Th release notes of SPSDK v1.10.1 (https://github.com/nxp-mcuxpresso/spsdk/releases/tag/1.10.0) includes this statement:

  • update PyOCD to latest version to support CMSIS DAP FW v3

Where can I find this "CMSIS DAP FW v3" ?

As far as I know, the latest (published) version of CMSIS-DAP is v2.1.1 (https://arm-software.github.io/CMSIS_5/DAP/html/dap_revisionHistory.html)

 

Tags (1)
0 Kudos
Reply
1 Solution
4,014 Views
marek-trmac
NXP Employee
NXP Employee

Hi Ivo,

see Software section for MCU LINK at: NXP web site 

Regards,
Marek


NOTE: If you find the answer useful, kindly click on [ACCEPT AS SOLUTION] button

View solution in original post

0 Kudos
Reply
2 Replies
4,015 Views
marek-trmac
NXP Employee
NXP Employee

Hi Ivo,

see Software section for MCU LINK at: NXP web site 

Regards,
Marek


NOTE: If you find the answer useful, kindly click on [ACCEPT AS SOLUTION] button
0 Kudos
Reply
4,004 Views
IvoBCD
Contributor III

OK, I see, so the release notes refer to MCU LINK FW v3, implementing CMSIS-DAP v2.1

 - V3.108 - Updates to CMSIS-DAP 2.1 and uses WinUSB for communication to host PC

, 

 

0 Kudos
Reply