CMSIS DAP FW v3 ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
3,956件の閲覧回数
IvoBCD
Contributor III

Th release notes of SPSDK v1.10.1 (https://github.com/nxp-mcuxpresso/spsdk/releases/tag/1.10.0) includes this statement:

  • update PyOCD to latest version to support CMSIS DAP FW v3

Where can I find this "CMSIS DAP FW v3" ?

As far as I know, the latest (published) version of CMSIS-DAP is v2.1.1 (https://arm-software.github.io/CMSIS_5/DAP/html/dap_revisionHistory.html)

 

タグ(1)
0 件の賞賛
返信
1 解決策
3,948件の閲覧回数
marek-trmac
NXP Employee
NXP Employee

Hi Ivo,

see Software section for MCU LINK at: NXP web site 

Regards,
Marek


NOTE: If you find the answer useful, kindly click on [ACCEPT AS SOLUTION] button

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
3,949件の閲覧回数
marek-trmac
NXP Employee
NXP Employee

Hi Ivo,

see Software section for MCU LINK at: NXP web site 

Regards,
Marek


NOTE: If you find the answer useful, kindly click on [ACCEPT AS SOLUTION] button
0 件の賞賛
返信
3,938件の閲覧回数
IvoBCD
Contributor III

OK, I see, so the release notes refer to MCU LINK FW v3, implementing CMSIS-DAP v2.1

 - V3.108 - Updates to CMSIS-DAP 2.1 and uses WinUSB for communication to host PC

, 

 

0 件の賞賛
返信