1 ROT+IMG key for MCXN546 Not Working

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

1 ROT+IMG key for MCXN546 Not Working

1,561件の閲覧回数
mosesrs
Contributor I

Hi,

I'm trying to build signed image for MCXN546 using NXP secure provisioning tool.

When I'm generating 4 ROT+IMG keys everything works well. However, when I'm using a single key, "Write Image" step fails. I suspect the tool generate wrong certificate block for images with single ROT+IMG keys.

mosesrs_0-1722169266627.png

 

Can you please verify this?

Thanks

0 件の賞賛
返信
2 返答(返信)

1,534件の閲覧回数
liborukropec
NXP Employee
NXP Employee

Hello Assaf,

I confirm this bug in the SEC v8, that is fixed in the upcoming v9 (stay tuned this week). The unused key slots must be configured in the CMPA - v9 takes the care, while in the v8 you have to do it manually in the RoTK_USAGE register:

liborukropec_0-1722242238257.png

 

I recommend to wait for SEC v9.

 

Using just 1 key seems like corner case and I'm interested about the use case; recommended is to use all 4 slots to be able do key revocation in the future.

Best regards,

Libor

0 件の賞賛
返信

1,557件の閲覧回数
mosesrs
Contributor I

Attached image is wrong. here is the correct screenshot:

mosesrs_0-1722169369027.png

 

0 件の賞賛
返信