1 ROT+IMG key for MCXN546 Not Working

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

1 ROT+IMG key for MCXN546 Not Working

1,928 次查看
mosesrs
Contributor I

Hi,

I'm trying to build signed image for MCXN546 using NXP secure provisioning tool.

When I'm generating 4 ROT+IMG keys everything works well. However, when I'm using a single key, "Write Image" step fails. I suspect the tool generate wrong certificate block for images with single ROT+IMG keys.

mosesrs_0-1722169266627.png

 

Can you please verify this?

Thanks

0 项奖励
回复
2 回复数

1,901 次查看
liborukropec
NXP Employee
NXP Employee

Hello Assaf,

I confirm this bug in the SEC v8, that is fixed in the upcoming v9 (stay tuned this week). The unused key slots must be configured in the CMPA - v9 takes the care, while in the v8 you have to do it manually in the RoTK_USAGE register:

liborukropec_0-1722242238257.png

 

I recommend to wait for SEC v9.

 

Using just 1 key seems like corner case and I'm interested about the use case; recommended is to use all 4 slots to be able do key revocation in the future.

Best regards,

Libor

0 项奖励
回复

1,924 次查看
mosesrs
Contributor I

Attached image is wrong. here is the correct screenshot:

mosesrs_0-1722169369027.png

 

0 项奖励
回复