tftp example to work with lwip

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

tftp example to work with lwip

3,010 Views
tbiberdorf
Contributor IV

In evaluating the lwip support by the MCUxpresso SDK provided by: Welcome to MCUXpresso | MCUXpresso Config Tools 

As part of the lwip support described, it states that lwip provides support for tftp but there is no demo code provided for tftp and the provided API for tftp will not work until a virtual file system is made available to support it.  I would have guessed that the SDK would have provided an example of how to implement this but they did not.

Can someone provide me a link or documentation on how to build the file system or better an example of how to generate the tftp communication?

thanks

Tags (1)
0 Kudos
Reply
1 Reply

2,109 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Terry,

I think that the LWIP supports tftp protocol, but we have ported the lwip source code to the UDP and TCP level, and we have developed the file system based on SDHC, but we have not the example code of  tftp example.

Hope it can help you

BR

XiangJun Rong

0 Kudos
Reply