lwip documentation for i.MXRT

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

lwip documentation for i.MXRT

ソリューションへジャンプ
2,757件の閲覧回数
nsiegel
Contributor V

Hi,

I'm looking for the lwip documentation.  I didn't find it in either the SDK or the SDK documentation package.  I'm most interested in the lwip version included with SDK v2.9.0 for iMXRT1170.

Thanks!

タグ(2)
0 件の賞賛
返信
1 解決策
2,728件の閲覧回数
PetrL
NXP Employee
NXP Employee

Hi, 

you can find the lwip version in the \middleware\lwip\ChangeLogKSDK.txt . There is specified exact branch and SHA which was used for given release. 

e.g :  

2.2.0_rev3
- Ported lwIP 2.2.0.dev (2020-07-07, branch: master, SHA-1: c385f31076b27efb8ee37f00cb5568783a58f299) to KSDK 2.0.0.

 

see:

https://git.savannah.nongnu.org/cgit/lwip.git/log/?qt=range&q=c385f31076b27efb8ee37f00cb5568783a58f2...

 

 

 

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,729件の閲覧回数
PetrL
NXP Employee
NXP Employee

Hi, 

you can find the lwip version in the \middleware\lwip\ChangeLogKSDK.txt . There is specified exact branch and SHA which was used for given release. 

e.g :  

2.2.0_rev3
- Ported lwIP 2.2.0.dev (2020-07-07, branch: master, SHA-1: c385f31076b27efb8ee37f00cb5568783a58f299) to KSDK 2.0.0.

 

see:

https://git.savannah.nongnu.org/cgit/lwip.git/log/?qt=range&q=c385f31076b27efb8ee37f00cb5568783a58f2...

 

 

 

0 件の賞賛
返信
2,744件の閲覧回数
nsiegel
Contributor V

Thank you for the link to the other post.  I noticed that post is from 2019, and refers to SDK v2.6.  Which version of lwip is included in SDK v2.9.0 for i.MXRT1170? 

What I'm really after is high level documentation of what's supported by the SDK.   Are there any release notes?  Are TLS, SSL, NTP, RTP/RTSP  supported?

Thanks  

0 件の賞賛
返信
2,752件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi,

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
To provide the fastest possible support, I'd highly recommend you refer to the post to learn the LwIP stack in the SDK library.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信