lpc5460x "Hello world vcom" sample problem on USB1

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

lpc5460x "Hello world vcom" sample problem on USB1

跳至解决方案
2,321 次查看
cybaluke
Contributor III

Hi, I'm working with the sample demo "lpcxpresso54608_hello_world_virtual_com" from SDK 2.4.0 with an LPC54608, I'm using MCUxpresso 10.2.0 and my board is the OM13092UL.

When I work on USB0 (on J3 FullSpd) the dbg console is routed on VCOM as I expected.

When I try to change the virtual com from USB0 to USB1 port (J2 HighSpd) changing the settings:

/*! @brief LPC USB IP3511 FS instance count */
#define USB_DEVICE_CONFIG_LPCIP3511FS (0U)

/*! @brief LPC USB IP3511 HS instance count */
#define USB_DEVICE_CONFIG_LPCIP3511HS (1U)

when I launch the debug session of the new code the host WIN10 O.S. get an error and it doesn't recognize the new virtual com device attached. What I'm missing to changing from USB0 to USB1 the VCOM on this sdk sample code?

Regards

标记 (4)
1 解答
1,699 次查看
miguel_mendoza
NXP Employee
NXP Employee

Hi cybaluke,

Apparently, the example "Hello world vcom" from the SDK, has some problems running with High Speed, as you say don't recognize the port, I recommended to use the "dev_cdc_vcom_bm" in the usb_examples section, this is very similar to the hello world example and run well with high speed, you only have to change the settings as you try before.

regards,
Miguel

在原帖中查看解决方案

2 回复数
1,700 次查看
miguel_mendoza
NXP Employee
NXP Employee

Hi cybaluke,

Apparently, the example "Hello world vcom" from the SDK, has some problems running with High Speed, as you say don't recognize the port, I recommended to use the "dev_cdc_vcom_bm" in the usb_examples section, this is very similar to the hello world example and run well with high speed, you only have to change the settings as you try before.

regards,
Miguel

1,699 次查看
cybaluke
Contributor III

... any idea or help about my issue?

0 项奖励
回复