flexio camera

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

flexio camera

Jump to solution
1,099 Views
seobi
Contributor III

Hi, We are planning to use a parallel camera with FlexIO on the EVKBRT1170.

Referring to the RT1010 sample, we have two questions during the implementation:

1. The PCLK on the RT1010 is said to support up to 20MHz. How much is supported in the case of the RT1170? I couldn't find this information in the datasheet.

2. The sample for the RT1010 is for 8-bit data, but in our case, we need to use 16-bit data. Is it possible to obtain a sample for this? If not, could you guide us on what needs to be modified?

Best regards,

0 Kudos
Reply
1 Solution
1,027 Views
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @seobi,

1. The PCLK frequency can be as high as the Clock Source frequency that the FlexIO admits. For the case of the RT1170, this would equate to a maximum of 120MHz.

2. I'm afraid that only 8-bit data is supported for the parallel camera emulated with FlexIO. I apologize for the inconvenience this may cause.

BR,
Edwin.

View solution in original post

0 Kudos
Reply
1 Reply
1,028 Views
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @seobi,

1. The PCLK frequency can be as high as the Clock Source frequency that the FlexIO admits. For the case of the RT1170, this would equate to a maximum of 120MHz.

2. I'm afraid that only 8-bit data is supported for the parallel camera emulated with FlexIO. I apologize for the inconvenience this may cause.

BR,
Edwin.

0 Kudos
Reply
%3CLINGO-SUB%20id%3D%22lingo-sub-1945760%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3Eflexio%20camera%3C%2FLINGO-SUB%3E%3CLINGO-BODY%20id%3D%22lingo-body-1945760%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3E%3CP%3EHi%2C%20We%20are%20planning%20to%20use%20a%20parallel%20camera%20with%20FlexIO%20on%20the%20EVKBRT1170.%3C%2FP%3E%3CP%3EReferring%20to%20the%20RT1010%20sample%2C%20we%20have%20two%20questions%20during%20the%20implementation%3A%3C%2FP%3E%3CP%3E1.%20The%20PCLK%20on%20the%20RT1010%20is%20said%20to%20support%20up%20to%2020MHz.%26nbsp%3B%3CSPAN%3EHow%20much%20is%20supported%20in%20the%20case%20of%20the%20RT1170%3F%20I%20couldn't%20find%20this%20information%20in%20the%20datasheet.%3C%2FSPAN%3E%3C%2FP%3E%3CP%3E2.%20The%20sample%20for%20the%20RT1010%20is%20for%208-bit%20data%2C%20but%20in%20our%20case%2C%20we%20need%20to%20use%2016-bit%20data.%20Is%20it%20possible%20to%20obtain%20a%20sample%20for%20this%3F%20If%20not%2C%20could%20you%20guide%20us%20on%20what%20needs%20to%20be%20modified%3F%3C%2FP%3E%3CP%3EBest%20regards%2C%3C%2FP%3E%3C%2FLINGO-BODY%3E%3CLINGO-SUB%20id%3D%22lingo-sub-1950374%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3ERe%3A%20flexio%20camera%3C%2FLINGO-SUB%3E%3CLINGO-BODY%20id%3D%22lingo-body-1950374%22%20slang%3D%22en-US%22%20mode%3D%22CREATE%22%3E%3CP%3EHi%26nbsp%3B%3CA%20href%3D%22https%3A%2F%2Fcommunity.nxp.com%2Ft5%2Fuser%2Fviewprofilepage%2Fuser-id%2F228348%22%20target%3D%22_blank%22%3E%40seobi%3C%2FA%3E%2C%3C%2FP%3E%0A%3CP%3E1.%20The%20PCLK%20frequency%20can%20be%20as%20high%20as%20the%20Clock%20Source%20frequency%20that%20the%20FlexIO%20admits.%20For%20the%20case%20of%20the%20RT1170%2C%20this%20would%20equate%20to%20a%20maximum%20of%20120MHz.%3C%2FP%3E%0A%3CP%3E2.%20I'm%20afraid%20that%20only%208-bit%20data%20is%20supported%20for%20the%20parallel%20camera%20emulated%20with%20FlexIO.%20I%20apologize%20for%20the%20inconvenience%20this%20may%20cause.%3C%2FP%3E%0A%3CP%3EBR%2C%3CBR%20%2F%3EEdwin.%3C%2FP%3E%3C%2FLINGO-BODY%3E