I noticed that a missing or bad I2C device causes MCU reset by watchdog. This is because of the infinite loop (Bold section in the code below) used in I2C driver functions such as:
1. I2C_MasterTransferNonBlocking() + I2C_MasterTransferAbort()
2. I2C_MasterTransferBlocking()
In the driver, if "I2C_RETRY_TIMES" defined, then it could get out the loop, see the code below.
#if I2C_RETRY_TIMES
uint32_t waitTimes = I2C_RETRY_TIMES;
/* Wait until bus not busy. */
while ((0U != (base->S & (uint8_t)kI2C_BusBusyFlag)) && (0U != --waitTimes))
{
}
if (0U == waitTimes)
{
result = kStatus_I2C_Timeout;
}
#else
/* Wait until data transfer complete. */
while (0U != (base->S & (uint8_t)kI2C_BusBusyFlag))
{
}
#endif
I do not want to add the definition in either fsl_i2c.h or fsl_common.h file, I am wondering if there is a driver configuration file, like FreeRTOSConfig.h for FreeRTOS for user to pass the configure information, or what is the best way to do so.
Regards.
解決済! 解決策の投稿を見る。
One way to do it as my colleague Kevin pointed out is to define that in Preprocessor, "I2C_RETRY_TIMES=3". It does work but place it into a file will be better.
Thanks Kevin.
One way to do it as my colleague Kevin pointed out is to define that in Preprocessor, "I2C_RETRY_TIMES=3". It does work but place it into a file will be better.
Thanks Kevin.
Yes. put the macros in Preprocessor is the right way.
Best reagards
Daniel