I noticed that a missing or bad I2C device causes MCU reset by watchdog. This is because of the infinite loop (Bold section in the code below) used in I2C driver functions such as:
1. I2C_MasterTransferNonBlocking() + I2C_MasterTransferAbort()
2. I2C_MasterTransferBlocking()
In the driver, if "I2C_RETRY_TIMES" defined, then it could get out the loop, see the code below.
#if I2C_RETRY_TIMES
uint32_t waitTimes = I2C_RETRY_TIMES;
/* Wait until bus not busy. */
while ((0U != (base->S & (uint8_t)kI2C_BusBusyFlag)) && (0U != --waitTimes))
{
}
if (0U == waitTimes)
{
result = kStatus_I2C_Timeout;
}
#else
/* Wait until data transfer complete. */
while (0U != (base->S & (uint8_t)kI2C_BusBusyFlag))
{
}
#endif
I do not want to add the definition in either fsl_i2c.h or fsl_common.h file, I am wondering if there is a driver configuration file, like FreeRTOSConfig.h for FreeRTOS for user to pass the configure information, or what is the best way to do so.
Regards.