Unable to import MCUXpresso SDK into MCUXpresso IDE

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Unable to import MCUXpresso SDK into MCUXpresso IDE

Jump to solution
458 Views
Abinandhan
Contributor I

I am trying to install the SDK for i.MX 8M Plus. For this, I have built and downloaded the SDK (SDK_25_03_00_EVK-MIMX8MP). While importing the SDK into MCUXpresso IDE v24.12.148, it is showing an error(mcuxpresso ide was unable to load one or more sdk(s). this may be because the sdk(s) was not created for the mcuxpresso ide or your ide is not up-to-date).

Below, I have mentioned the steps that I followed. Kindly help to resolve this issue.

Step 1: Selected the i.MX8MP at the board selection in MCUXpresso SDK Builder and built the SDK.

Abinandhan_0-1745236837641.png

Abinandhan_1-1745237668087.png

Abinandhan_2-1745237809919.pngAbinandhan_3-1745237889273.pngAbinandhan_4-1745237940870.png

Step 2: After downloading the SDK, I opened the MCUXpresso IDE > Installed SDKs, and dragged and dropped the .zip SDK file into the Installed SDKs section. After that, an error window popped up. I have attached the screenshot of it.

Abinandhan_5-1745238224128.pngAbinandhan_6-1745238273646.png

Kindly help to resolve this issue.

0 Kudos
Reply
1 Solution
434 Views
Chavira
NXP TechSupport
NXP TechSupport

Hi @Abinandhan!

Thank you for contacting NXP Support!

 

Unfortunately MCUXpresso IDE is not compatible with the SDK of iMX processors.

You can follow the AN14120 to compile and debug the iMX8MP using IAR IDE or Visual Code.

 

Best Regards!

Chavira

View solution in original post

0 Kudos
Reply
1 Reply
435 Views
Chavira
NXP TechSupport
NXP TechSupport

Hi @Abinandhan!

Thank you for contacting NXP Support!

 

Unfortunately MCUXpresso IDE is not compatible with the SDK of iMX processors.

You can follow the AN14120 to compile and debug the iMX8MP using IAR IDE or Visual Code.

 

Best Regards!

Chavira

0 Kudos
Reply