USB device RNDIS on iMX RT1176

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB device RNDIS on iMX RT1176

3,712件の閲覧回数
zachyu
Contributor I

I want to find some SDKs which demonstrates how to setup USB device RNDIS using lwip and FreeRTOS on  iMX RT1176. The data throughput between iMX RT1176 and PC can reach 16MB per second. It seems that the latest MCUXpresso dose not include such example.

0 件の賞賛
返信
5 返答(返信)

3,681件の閲覧回数
DanielRuvalcaba
NXP TechSupport
NXP TechSupport

Hi,

Could you please take a look to the MCUXpresso SDK USB RNDIS & LWIP User Guide and the lwip_dhcp_usb SDK demo?

I believe this might help you with your query.

Best regards, Daniel.

0 件の賞賛
返信

3,671件の閲覧回数
zachyu
Contributor I

Dear Daniel,

The MCUXpresso SDK USB RNDIS & LWIP User Guide and the lwip_dhcp_usb SDK demo is based on USB Host RNDIS. I studied the source file of usb_ethernetif_freertos.c. There are two threads that handle usb event and data communication. The interface and callback functions tightly dependent on usb host core and class functions. I think the task migrating usb host RNDIS to device RNDIS is very complex for me. On the other hand, The MCUXpresso SDK usb_device_cdc_vnic demo is useful reference. I plan to add LWIP tcp/ip stacks to usb vnic. Do you think this is an easier option?

After all, I hope The MCUXpresso SDK provide USB device RNDIS&LWIP.

0 件の賞賛
返信

3,646件の閲覧回数
DanielRuvalcaba
NXP TechSupport
NXP TechSupport

Unfortunately, I´m not able to tell you a "best" way to achieve this since we don’t have a guide or tutorial on how to do this.

I´m sorry for the inconvenience this might cause you.

Best regards, Daniel.

0 件の賞賛
返信

3,532件の閲覧回数
zachyu
Contributor I

Finally I succeed to realize USB device RNDIS function based on the demo of usb_device_cdc_vnic. The data throughput about 120Mbps is obtained. I think the throughput may be optimized at some extend. 

0 件の賞賛
返信

3,196件の閲覧回数
mbora
Contributor III

Hi! I'm glad that you managed to make it work. Could you leave some tips on your "journey" to making it work? I myself now struggle to do it, so I would be very grateful. Thanks!

0 件の賞賛
返信