Hi experts,
I already post over a reply on this topic at this link, but probably went lost inside the old answers, so I rewrite it here.
I'm using the latest MCUXpresso 11.3.0.
I installed the SDK_2.9.0_FRDM-K64F for which I'd like to access to the API documentation.
I can open the SDK Getting started or the Release notes from:
- within the MCUXpresso IDE or
- from the docs folder inside the SDK or
- from the SDK web page

Unfortunately none of the 3 above point me to the SDK documentation. I found "something" just using Google a this address but of course I think there is a better way to access to the official documentation. What is it?
One more, I think that would be very appreciated been able to open the SDK html (exist?!?) from within the MCUXpresso IDE.
Would be also very useful use the context menu over a function to open directly the function doc (I suppose the SDK is done with the Doxygen).
Any help would be very appreciated! Many thanks!
Kind regards,
AGA