SDK documentation

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SDK documentation

Jump to solution
21,359 Views
superaga
Contributor III

Hi experts,

I already post over a reply on this topic at this link, but probably went lost inside the old answers, so I rewrite it here.

 

I'm using the latest MCUXpresso 11.3.0.

I installed the SDK_2.9.0_FRDM-K64F for which I'd like to access to the API documentation.

I can open the SDK Getting started or the Release notes from:

  • within the MCUXpresso IDE or
  • from the docs folder inside the SDK or
  • from the SDK web page

 

superaga_0-1613453782226.png

 

Unfortunately none of the 3 above point me to the SDK documentation. I found "something" just using Google a this address but of course I think there is a better way to access to the official documentation. What is it?

One more, I think that would be very appreciated been able to open the SDK html (exist?!?) from within the MCUXpresso IDE.

Would be also very useful use the context menu over a function to open directly the function doc (I suppose the SDK is done with the Doxygen).

 

Any help would be very appreciated! Many thanks!

Kind regards,

AGA

0 Kudos
Reply
1 Solution
21,304 Views
danielholala
Senior Contributor II

Hi AGA,

the link you posted points to a "API Reference Manual" in PDF format.

I think that this PDF document contains information very similar to what is provided on https://mcuxpresso.nxp.com/en/apidoc/  (created from doxygen comments, or so it seems).

Just checked for "MK64FN1M0xxx12" (this might not be exactly your processor) that is to be found here:

https://mcuxpresso.nxp.com/api_doc/dev/2117/

What do you think?

 

 

View solution in original post

5 Replies
21,305 Views
danielholala
Senior Contributor II

Hi AGA,

the link you posted points to a "API Reference Manual" in PDF format.

I think that this PDF document contains information very similar to what is provided on https://mcuxpresso.nxp.com/en/apidoc/  (created from doxygen comments, or so it seems).

Just checked for "MK64FN1M0xxx12" (this might not be exactly your processor) that is to be found here:

https://mcuxpresso.nxp.com/api_doc/dev/2117/

What do you think?

 

 

21,292 Views
superaga
Contributor III

Hi @danielholala,

this is exactly what I was looking for!

In fact this, respect the one that I found (PDF), has more details (since it is generated by the function itself) and also more navigable (because the hyperlinks).

It is a shame that this page (the main or the related to the processor) is not directly accessible from the MCUXpresso IDE, that would be super useful.

I think also that NXP should easily provide this link from the main SDK page. May be it's my mistake, but I couldn't find it...

 

Many thanks to all!

Regards,

AGA

21,332 Views
superaga
Contributor III

Hi @danielchen,

many thanks for your answer.

I didn't have the documentation since I installed the SDK from within MCUXpresso IDE (as in this guide).

Is there a way to download it from the IDE?

One suggestion: would be very useful to access the API documentation from the IDE itself, "like the tooltips when hovering the mouse on code".

 

Best regards,

AGA

0 Kudos
Reply
21,314 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi @superaga 

 

Thank you for your good suggestions.

Currently SDK documents are downloaded from mcuxpresso.com .  I also attached API doc here.

I will report your suggestion to the SDK team.

 

Regards

Daniel

21,328 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi @superaga ;

 

Please download the SDK documentation from 

https://mcuxpresso.nxp.com/en/welcome

when you download the SDK.

danielchen_0-1613539499758.png

Regards

Daniel

 

0 Kudos
Reply