RTOS heap files

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

RTOS heap files

跳至解决方案
2,279 次查看
danielkrol
Contributor III

Hi,
I have a problem when creating a new project with Free RTOS in SDK 2.14.0 and 2.15.0 for MCU (e.g. LPC55s69). No heap files are created in the MemMang folder - which causes errors:

Zrzut ekranu 2024-02-27 o 16.22.29.png

In earlier versions (up to 2.13.1), heap files were automatically created: 

Zrzut ekranu 2024-02-27 o 16.23.04.png

If I import some RTOS example from SDK 2.15.0, the heap files are there. The problem only occurs when creating a new project.

Is this some kind of SDK manager error?

 

Regards,

Daniel

0 项奖励
回复
1 解答
2,179 次查看
Harry_Zhang
NXP Employee
NXP Employee

@danielkrol 

I can reproduce this issue, and I will report this issue to our SDK team.

Thank you for the information.

Best regards,
Hang

在原帖中查看解决方案

4 回复数
2,196 次查看
Harry_Zhang
NXP Employee
NXP Employee

Hi @danielkrol 

I imported freerots_sme example from 2.14 and 2.15 SDK using MCUXpresso and IAR IDE, and there are heap_4.c files inside, so the problem that you mentioned did not occur, so please check it again.

Best regards,
Hang

 

0 项奖励
回复
2,191 次查看
danielkrol
Contributor III

Hi,

Yes, it is in the examples. However, the problem occurs if you create a NEW project for RTOS - there is no heap file.

 

Regards,

Daniel

0 项奖励
回复
2,180 次查看
Harry_Zhang
NXP Employee
NXP Employee

@danielkrol 

I can reproduce this issue, and I will report this issue to our SDK team.

Thank you for the information.

Best regards,
Hang

2,175 次查看
danielkrol
Contributor III

Hi,

Thank you so much!

Regards,
Daniel

0 项奖励
回复