RTOS heap files

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RTOS heap files

Jump to solution
2,268 Views
danielkrol
Contributor III

Hi,
I have a problem when creating a new project with Free RTOS in SDK 2.14.0 and 2.15.0 for MCU (e.g. LPC55s69). No heap files are created in the MemMang folder - which causes errors:

Zrzut ekranu 2024-02-27 o 16.22.29.png

In earlier versions (up to 2.13.1), heap files were automatically created: 

Zrzut ekranu 2024-02-27 o 16.23.04.png

If I import some RTOS example from SDK 2.15.0, the heap files are there. The problem only occurs when creating a new project.

Is this some kind of SDK manager error?

 

Regards,

Daniel

0 Kudos
Reply
1 Solution
2,168 Views
Harry_Zhang
NXP Employee
NXP Employee

@danielkrol 

I can reproduce this issue, and I will report this issue to our SDK team.

Thank you for the information.

Best regards,
Hang

View solution in original post

4 Replies
2,185 Views
Harry_Zhang
NXP Employee
NXP Employee

Hi @danielkrol 

I imported freerots_sme example from 2.14 and 2.15 SDK using MCUXpresso and IAR IDE, and there are heap_4.c files inside, so the problem that you mentioned did not occur, so please check it again.

Best regards,
Hang

 

0 Kudos
Reply
2,180 Views
danielkrol
Contributor III

Hi,

Yes, it is in the examples. However, the problem occurs if you create a NEW project for RTOS - there is no heap file.

 

Regards,

Daniel

0 Kudos
Reply
2,169 Views
Harry_Zhang
NXP Employee
NXP Employee

@danielkrol 

I can reproduce this issue, and I will report this issue to our SDK team.

Thank you for the information.

Best regards,
Hang

2,164 Views
danielkrol
Contributor III

Hi,

Thank you so much!

Regards,
Daniel

0 Kudos
Reply