Need clarification on USB g_compositeDeviceConfigList.count

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Need clarification on USB g_compositeDeviceConfigList.count

1,650 Views
michaelhuslig
Contributor IV

The MCUXpresso SDK USB Stack Composite Device User's Guide, section 4.2, says the config list count should be the number of classes in the composite device.  It shows as example MSD+CDC is 2 classes.

Shouldn't CDC+CDC be 1 class?  The SDK example twrk22f120m_dev_composite_cdc_vcom_cdc_vcom_freertos shows it as 2.

0 Kudos
Reply
1 Reply

1,524 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi MICHAEl:

CDC+CDC is two classes, usb stack will need allocate more memory. You can consider it as the count of classes rather than the type of  classes.

Regards

Daniel

0 Kudos
Reply