Hi @Alice_Yang ,
Thank you for your response. I know that there is no demo board for the LPC5526.
Yes, I want to use the example code for LPC55S28 on LPC5526 and change GPIOs, UART, etc so the code works with my own board.
As I mentioned, there is example code included in the LPC5526 SDK for LPCxpresso55S28 demo board, see below:
LPC5526 SDK
However, the "Import SDK example(s)" wizard does not show the board when clicking on LPC5526. I consider this a bug!
Workaround:
To select the board, click on LPC55S28. This makes two lpcxpresso55S28 demo boards appear. Now select the board that has the LPC5526 SDK associated with it.
Import SDK Examples Wizard