Cypress WICED WiFi Stack removed from SDK 2.10.0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Cypress WICED WiFi Stack removed from SDK 2.10.0

1,697 Views
phaggren
Contributor I

Hello NXP!

 

I noticed that you have removed the Cypress WICED WiFi support from your latest SDK 2.10.0, at least on the iMX-RT 1064 package.

I can only see support for the NXP's own WiFi modules.

 

Why is that?

Are there any issues with new SDK and the WICED code?

 

My current WICED code runs and compiles with the new SDK but need to do more testing.

 

Hopefully this is just temporary as the Murata's WiFi modules are important to many of us.

 

All the best

Petri

 

 

0 Kudos
Reply
1 Reply

1,691 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @phaggren 

  The new SDK mainly support the NXP's WIFI chip from SDK2.10.0, and remove the old cypress wifi code.

  If you need the cypress wifi examples, you can refer to the old SDK2.9.2, which still can be downloaded from this link:

https://mcuxpresso.nxp.com/en/builder?hw=EVK-MIMXRT1064&rel=467

 

Wish it helps you!
Best Regards,

Kerry

 

0 Kudos
Reply