K22F IAR Fatal error[Pe035]

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

K22F IAR Fatal error[Pe035]

2,132 次查看
oswaldo-153
Contributor III
Hello
I have a question
I am working with IAR, it generates an error, where I can define my micro controller MK22FN128VLL10 and how to do it, I thank you very much
标签 (1)
2 回复数

2,062 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Oswaldo Tovar,

Please find the MK22F12810 related files in MCUXPresso SDK folder(...\SDK_2.6.0_MK22FN128xxx10\devices\MK22F12810)

devices MK22F12810.png
CPU_MK22FN128VLL10 should define in Defined symbols.

Defined symbols CPU_MK22FN128VLL10.png

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,062 次查看
oswaldo-153
Contributor III

thank you, novice

I am trying to edit the clock_config file to manually select which clock source will be used. 
In other words, I will write conditions in the clock_config file to have options from the different clock sources.
I'm supporting MCUXpresso, but there are many variables to modify, edit modes of operation, dividers and more
I'm not sure if the file fsl_clock are those condition, thank you.
0 项奖励
回复