K22F IAR Fatal error[Pe035]

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

K22F IAR Fatal error[Pe035]

2,140件の閲覧回数
oswaldo-153
Contributor III
Hello
I have a question
I am working with IAR, it generates an error, where I can define my micro controller MK22FN128VLL10 and how to do it, I thank you very much
ラベル(1)
2 返答(返信)

2,070件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Oswaldo Tovar,

Please find the MK22F12810 related files in MCUXPresso SDK folder(...\SDK_2.6.0_MK22FN128xxx10\devices\MK22F12810)

devices MK22F12810.png
CPU_MK22FN128VLL10 should define in Defined symbols.

Defined symbols CPU_MK22FN128VLL10.png

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,070件の閲覧回数
oswaldo-153
Contributor III

thank you, novice

I am trying to edit the clock_config file to manually select which clock source will be used. 
In other words, I will write conditions in the clock_config file to have options from the different clock sources.
I'm supporting MCUXpresso, but there are many variables to modify, edit modes of operation, dividers and more
I'm not sure if the file fsl_clock are those condition, thank you.
0 件の賞賛
返信