Fatfs: lost space in multipartition?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Fatfs: lost space in multipartition?

709件の閲覧回数
biafra
Senior Contributor I

Hi everyone,

I'm using MCUXpresso 10.2.1 and a custom board based on MK66F2M0

I'm using a 4 MB dataflash partioned in two disks using 512 bytes sector size:

DWORD plist[] = { 6894, 1008, 0, 0}; /* Divide drive into two partitions */

f_fdisk( 5, plist, FormatBuf ); //create partitions

I can access both disks, but it seems that the disk sizes are wrong: with the f_getfree() function I get 2768 kB and 456 kB respectively.

res = f_getfree( DiskName, &fre_clust, &fs );
if( res == FR_OK )
{
   /* Get total sectors */
   tot_sect = ( fs->n_fatent - 2 ) * fs->csize;
   ...
}

Why is there such a waste of space?

Many thanks
Biafra

0 返答(返信)