Eclipse Marketplace Client

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Eclipse Marketplace Client

Jump to solution
6,605 Views
driesmoors
NXP Employee
NXP Employee

Hi,

How can I install the Eclipse Marketplace Client in MCUXpresso? It is not available by default under Help > Install new software... 

After adding the repository http://download.eclipse.org/mpc/neon, I can select the plugin, but installation cannot be completed due to a missing requirement:

Cannot complete the install because one or more required items could not be found.
Software being installed: Marketplace Client 1.5.1.v20160929-1432 (org.eclipse.epp.mpc.feature.group 1.5.1.v20160929-1432)
Missing requirement: Marketplace Client 1.5.1.v20160929-1432 (org.eclipse.epp.mpc.feature.group 1.5.1.v20160929-1432) requires 'org.eclipse.equinox.p2.discovery.feature.feature.group [1.0.0.v201004,2.0.0)' but it could not be found

What other repositories need to be added, and which plugins need to be minimally installed?

Thanks,
Dries.

Labels (1)
Tags (1)
1 Solution
4,708 Views
scaggsp
Contributor II

Try installing from the releases repository.

http://download.eclipse.org/releases/neon

The Eclipse Marketplace Client is under General Purpose Tools → Marketplace Client

View solution in original post

2 Replies
4,709 Views
scaggsp
Contributor II

Try installing from the releases repository.

http://download.eclipse.org/releases/neon

The Eclipse Marketplace Client is under General Purpose Tools → Marketplace Client

4,709 Views
driesmoors
NXP Employee
NXP Employee

Thanks, that worked.

Any reason why the Neon release repo is not included by default? And why the Marketplace is not installed by default?