Do you have the startup code for configuring DA7212 codec on FRDM K66 board?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Do you have the startup code for configuring DA7212 codec on FRDM K66 board?

Jump to solution
3,837 Views
vishnusasidhara
Contributor I

So far, this is what I have tried:

main()

{

I2C_MasterTransferCreateHandle(I2C0, &g_m_handle, i2c_master_callback, NULL);

readcodec();

}

readcodec()

{

uint8_t data[2];

i2c_master_config_t masterConfig;

I2C_MasterGetDefaultConfig(&masterConfig);

masterConfig.baudRate_Bps = I2C_BAUDRATE;

sourceClock = CLOCK_GetFreq(I2C0_CLK_SRC);

I2C_MasterInit(I2C0, &masterConfig, sourceClock);

i2c_master_transfer_t masterXfer;
memset(&masterXfer, 0, sizeof(masterXfer));

masterXfer.slaveAddress = 0x1AU;
masterXfer.direction = kI2C_Read;
masterXfer.subaddress = 0x2;
masterXfer.subaddressSize = 0;
masterXfer.data = &data;
masterXfer.dataSize = 1;
masterXfer.flags = kI2C_TransferNoStopFlag;

I2C_MasterTransferNonBlocking(I2C0, &g_m_handle, &masterXfer);

/* wait for transfer completed. */
while ((!nakFlag) && (!completionFlag))
{
}

nakFlag = false;

if (completionFlag == true)
{
completionFlag = false;
find_device = true;
}
}

This is based out of the Accelerometer demo application that was part of the KSDK bundle.

I am trying to read DA7212's status register. So far, no I2C interrupt itself is getting generated, and the code is stuck at while(!nakFlag). Please help.

Is there a sample application for using DA7212 in the FRDM K66 board?

0 Kudos
Reply
1 Solution
3,371 Views
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Vishnu S

Please download SDK 2.x in the SDK builder here:

Welcome to MCUXpresso | MCUXpresso Config Tools 

If you have problems with the download, please check this link:

https://community.nxp.com/docs/DOC-333304 

Best Regards

Jorge Alcala

View solution in original post

0 Kudos
Reply
4 Replies
3,371 Views
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Vishnu S

You could use drivers provided in SDK package, the demo example code and de drivers example code of SAI module have file named fsl_dialog7212.c . Please check this examples codes inside the path <SDK_2.2_FRDM-K66F>\boards\frdmk66f\driver_examples\sai\.

Hope this information could help you.

Best Regards

Jorge Alcala

0 Kudos
Reply
3,371 Views
vishnusasidhara
Contributor I

Hi Jorge,

Thank you for your response.

I am using SDK 2.0 and doesn't have this folder under driver_examples. I am able to find only SDK 2.0 and WolfSSL for Kinetis under www.nxp.com/ksdk. Can you please help me with the link to this SDK 2.2 download?

Thanks.

0 Kudos
Reply
3,372 Views
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Vishnu S

Please download SDK 2.x in the SDK builder here:

Welcome to MCUXpresso | MCUXpresso Config Tools 

If you have problems with the download, please check this link:

https://community.nxp.com/docs/DOC-333304 

Best Regards

Jorge Alcala

0 Kudos
Reply
3,371 Views
vishnusasidhara
Contributor I

Thanks Jorge. I was able to download the SDK and it solved the issues. My codec is up. Sorry for the delay in response.

0 Kudos
Reply