DebugConsole adds 'swo' but files are missing

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DebugConsole adds 'swo' but files are missing

2,021 Views
ingenutec
Contributor III

The v2.5 SDK adds SERIAL_PORT_TYPE_SWO as an output option, but if this is defined, then serial_manager.h attempts to include serial_port_swo.h which does not exist in the SDK.

This is also not in the current documentation.  Is this a work in progress?

Are there any plans to add SEGGER_RTT as an output option in the DebugConsole?

Thanks,

Robert Palmer

0 Kudos
Reply
4 Replies

1,933 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi robert palmer,

  Please check the attached swo files.

  You can unzip it, then put the files in folder: SDK_2.6.0_FRDM-K82F\components\serial_manager

  You can try it on your side.

 

Have a great day,
Kerry

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

1,933 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi robert palmer ,

  Please tell me which detail SDK you are using? Tell me the kinetis chip part number.

  I will check it, and report it to our SDK department.

 


Have a great day,
Kerry

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

1,933 Views
ingenutec
Contributor III

I'm looking at the MK8x family SDK for Mac, Linux and Windows.

0 Kudos
Reply

1,933 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi robert palmer,

  I have reproduce the problem which you mentioned, I will help you to report it to our SDK department.

Have a great day,
Kerry

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply