Changelog for MCUXpresso SDK v24.12.0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Changelog for MCUXpresso SDK v24.12.0

1,827 Views
zenghuchen
Contributor II

Hi,

It is great to see a new MCUXpresso SDK release.

However, I cannot find the changelog by comparison to previous one (SDK_2.14.0_EVK-MIMXRT595). And from release documentation (https://mcuxpresso.nxp.com/mcuxsdk/latest/html/release/index.html) there is little information.

BR

Jack

0 Kudos
Reply
5 Replies

1,803 Views
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @zenghuchen,

The Github changelog can be found on the following link: https://github.com/nxp-mcuxpresso/mcuxsdk-manifests/compare/24.12.00-pvw2_POST_1216...v24.12.00

You can also find the driver changelog for each RT500 part on the following path: "<SDK repo installation path>\devices\RT\RT500\MIMXRT595S\drivers\ChangeLogKSDK.txt".

BR,
Edwin.

0 Kudos
Reply

1,736 Views
zenghuchen
Contributor II

Thanks @EdwinHz,

But the first link points to commits. This is too granular. Is there a high-level overview?

The driver ChangeLog is very useful. But unfortunately, I cannot find them in the provided path. Are you able to share them directly or attach them to github?

Thanks

Jack 

0 Kudos
Reply

1,723 Views
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @zenghuchen,

I have attached the ChangeLogKSDK.txt file for the latest SDK version of RT500.

BR,
Edwin.

0 Kudos
Reply

1,665 Views
zenghuchen
Contributor II

Hi EdwinHz,

The changelog seems to be incomplete. For example, I noticed fsl_i3c driver has upgraded from 2.10.3 to 2.13 but this is not documented in the attached log. Same to some other drivers.

BR

Zenghu Chen

0 Kudos
Reply

1,644 Views
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @zenghuchen,

That's all that we have to share as the changelog for the latest version of the SDK. Sorry for the inconvenience this may cause.

 

 

0 Kudos
Reply