Bug in lpspi driver?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Bug in lpspi driver?

Jump to solution
1,597 Views
imxrtuser
Senior Contributor I

Hello,

I was just testing the LPSPI driver and realized that the clock cycles in register LPSPI1>SCKPCS, PCSSCK and DBT get set wrong. I think there is a bug in the function LPSPI_MasterSetDelayTimes of the fsl_lpspi.c SDK driver.

I am using SDK_2.7.0_EVK-MIMXRT1020_FreeRTOS with fsl_lpspi driver version

#define FSL_LPSPI_DRIVER_VERSION (MAKE_VERSION(2, 0, 4))

If you look at the function the variable realDelay is of type uint32_t. On line 658 of fsl_lpspi.c the variable gets set to

realDelay = 1000000000U;

which is roughly maximum value of uint32_t divided by four and on line 659 realDelay gets multiplied by the scaler plus some offset

realDelay *= (scaler + 1U + additionalScaler);

The scaler will start with 0 and go up to 255 which will result in too large data.

If I change the data type of realDelay (and I think the same problem is true for bestDelay) to uint64_t I get the correct result. Is this enough or do I have to change anything else?

Kind regards,

Stefan

0 Kudos
Reply
1 Solution
1,498 Views
FelipeGarcia
NXP Employee
NXP Employee

Hello Stefan,

 

You are correct, this issue will be reported for the next version of SDK. You can also refer to this thread: LPSPI Delay calculation error (fsl_lpspi.c - v2.7.0) 

 

Thanks for your feedback!


Have a great day,
Felipe

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
1,499 Views
FelipeGarcia
NXP Employee
NXP Employee

Hello Stefan,

 

You are correct, this issue will be reported for the next version of SDK. You can also refer to this thread: LPSPI Delay calculation error (fsl_lpspi.c - v2.7.0) 

 

Thanks for your feedback!


Have a great day,
Felipe

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply
1,498 Views
imxrtuser
Senior Contributor I

Thank you Felipe!

Kind regards,

Stefan

0 Kudos
Reply