I upgraded from MCUXpresso SDK 2.6.2. to 2.7.0 and now usb_usrt_drv.c fails to compile because fsl_uart,h is missing and many definitions like uart_handle_t, UART_TYPE, UART_BASE_PTRS, and others along with it. Is there an updated usb_uart_drv.c?
Hello Jeff Thompson
The driver for the uart is called fsl_lpuart. Also the uart.h can be found at the components folder. You can drag these files from the sdk folder to your project.
If you have more questions do not hesitate to ask me.
Best regards,
Omar
Hello Jeff Thompson
Can you help me providing me the part number of the device you are working with?
Best regards,
Omar
Omar,
It’s the MIMXRT1062DVL6A.
Jeff Thompson | Senior Electrical Engineer-Firmware
+1 704 752 6513 x1394