BLE Mesh library.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

BLE Mesh library.

3,473件の閲覧回数
robertkonc
Contributor II

When we could expext SDK 2.3 for KW41?

Or, when BLE mesh library will be available?

Best regards,

Robert

4 返答(返信)

3,150件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Robert.

I was informed there is no plan to create BLE mesh library for KW41 in recent road map.

I will let you know the expect release time of SDK 2.3 for KW41 if I get feedback.


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

3,150件の閲覧回数
thomasblank
Contributor II

At Bluetooth Smart / Bluetooth Low Energy (BLE)|NXP  It is said that the KW41Z already supports the BLE Mesh topology. Which information is accurate now?

0 件の賞賛
返信

3,150件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Thomas.

You are right KW41 support BLE Mesh, but our SDK doesn't have support for it.

I got latest news from KW41 PM  there are no plans to support this version SDK2.3.

Have a great day,
Jennie Zhang

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

3,150件の閲覧回数
pucher
Contributor I

Hi Jennie,

in the Kinetis BLE Software V1.2.2, there is a BLE Mesh Library along with some examples.

Would you recommend to build a mesh application on top of that library? Or is it already outdated and not recommended to use?

Best Regards

Christian

0 件の賞賛
返信