mcuxpresso debug flash

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

mcuxpresso debug flash

3,415件の閲覧回数
paul_roberts
Contributor III

I'm working with Kinetis K22F Freedom Board.  After I convert my .axf output file to .s19, I append a CRC32 value to the s-record, then convert the .s19 file to .bin.  When I debug, I would like to program flash using either the .s19 or the .bin file which contain the appended CRC32 vale, so that I can see it when I view memory in the debugger, and I can debug my CRC32 algorithm.  I can see that the original .axf file is essentially a binary file with debug information in it.  How can I would like to force the debugger to program flash a different output file so that this gets done.  Any suggestions are much appreciated! Cheers. Paul.

0 件の賞賛
返信
2 返答(返信)

3,137件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi Paul,

my suggestion would be to program it with the 'Program to flash' function, see Using Eclipse to Program Binary Files to an Embedded Target | MCU on Eclipse 

Then you still can debug it: for this, only use the symbols in the debug configuration without loading the binary. Or use the 'attach' functionality, see 'attaching' in Overview of MCUXpresso IDE v10.2.0 | MCU on Eclipse 

I hope this helps,

Erich

0 件の賞賛
返信

3,136件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Paul Roberts ,

How about first download the s19 file:

pastedImage_1.png

then using "Connectin to a running Target (attach)" to debug it , about the detail please have a look at

11.3.2 Connecting to a running Target (attach) of <MCUXpresso_IDE_User_Guide.pdf> .


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信