installing MCUExpresso IDE under openSuSE

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

installing MCUExpresso IDE under openSuSE

ソリューションへジャンプ
2,802件の閲覧回数
ve3id
Contributor IV

I made the tactical error of upgrading mcuexpressoide from 11.8.1 to 11.9.0  in the middle of a project, hoping it would resolve some minor issues.

I know the deb.bin file is for debian-based systems, but it has been installing fine on my openSuSE Leap 15.3 and 15.4 for a year or two now, since ide  11.5 in fact.

So I downloaded the update and installed it, replacing 11.8.1.  At first it worked no problem, but after a reboot, it cannot find the binary.  Nor can I find it manually.

So I tried installing again (11.9.0 over 11.9.0) and 1) it failed to find libc6, which I expect since it should use glibc, and dozens of dependencies not met. That should only affect jlink, which I do not use.

I can't understand how 11.5 and 11.8 could have loaded fine (and let me get thousands of lines into my project) and not now.  I reasoned that there must be a symlink missing, but no idea what or where!

Has anybody else experienced this?

Any help really appreciated.

cheers,

Nigel Johnson

 

0 件の賞賛
返信
1 解決策
2,780件の閲覧回数
ve3id
Contributor IV

Solved!  After installing an upgrade to openSuSE Linux Leap 15.5 and doing the 781 updates, I was hoping that an appropriate path or link was re-set, still Nothing.  Then I installed the full generic Eclipse C development system.  Ran it again, and it did install the files but no menu entry, but that was easy to fix.

 

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,781件の閲覧回数
ve3id
Contributor IV

Solved!  After installing an upgrade to openSuSE Linux Leap 15.5 and doing the 781 updates, I was hoping that an appropriate path or link was re-set, still Nothing.  Then I installed the full generic Eclipse C development system.  Ran it again, and it did install the files but no menu entry, but that was easy to fix.

 

0 件の賞賛
返信
2,801件の閲覧回数
ve3id
Contributor IV

I should add that I went back and tried to re-install 11.8 with the same errors 

0 件の賞賛
返信