#include-ing and linking against a library project automatically?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

#include-ing and linking against a library project automatically?

2,282 次查看
Slaymaker
Contributor III

Is there a way to configure a library project to export a #include path, library search path, and library name so that just adding it as a dependency to another project (lib or executable) will automatically add that path and name to the dependent project?

I ask because I've gotten it working by manually adding the #include path, libpath, and name, but I'm wondering if I misconfigured the library project somehow because I've seen other IDEs that can do that (and implemented it in a another custom multi-project build system).

Thanks!

0 项奖励
回复
4 回复数

2,206 次查看
lpcxpresso_supp
NXP Employee
NXP Employee

See [1] for some automation around linking projects to libraries. Is the "Smart Update" wizard what you're looking for?

Regards,
MCUXpresso IDE Support

[1] https://community.nxp.com/t5/LPCXpresso-IDE-FAQs/Creating-and-Linking-to-Library-Projects/m-p/469212

 

0 项奖励
回复

2,255 次查看
Slaymaker
Contributor III

Thanks, but that's how to manually configure it seemingly to work around an IDE bug.

I'm trying to see if this IDE can automatically configure it, like other IDEs can.

0 项奖励
回复

2,240 次查看
ErichStyger
Specialist I

I don't think what you mean or want is coming from the IDE, but from the build system?

So you simply might use CMake for this?

0 项奖励
回复

2,272 次查看
ErichStyger
Specialist I
0 项奖励
回复