errors in build example by MCUXpresso IDE

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

errors in build example by MCUXpresso IDE

4,751件の閲覧回数
1901167646
Contributor II

 when in build the exampe the MCUXpresso IDE worse error ,butthe example is from the Official routine which i download from NXP

the errors are:

  描述 资源 路径 位置 类型
D:\KW41Z\MCUXpressoIDE_10.2.0_759\ide\msys\bin\make.exe: *** Couldn't reserve space for cygwin's heap, Win32 error 0 usbkw41z_kw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos C/C++ Problem
first defined here semihost_hardfault.c /usbkw41z_kw41z_1wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_usbkw41z_kw41z_1/source 第 73 行 C/C++ Problem
make: *** [source/common/ble_conn_manager.o] Error 1 projectwireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_projict C/C++ Problem
make: *** [source/common/gatt_db/gatt_database.o] Error 1 projectwireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_projict C/C++ Problem
make: *** [usbkw41z_kw41z_1wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_usbkw41z_kw41z_1.axf] Error 1 usbkw41z_kw41z_1wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_usbkw41z_kw41z_1 C/C++ Problem
make: *** [utilities/fsl_debug_console.o] Error 1 projectwireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_projict C/C++ Problem
make: *** Waiting for unfinished jobs.... projectwireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_projict C/C++ Problem
multiple definition of `HardFault_Handler' debug_log.c /usbkw41z_kw41z_1wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos_usbkw41z_kw41z_1/nwk_ip/base/utils 第 515 行 C/C++ Problem

タグ(1)
7 返答(返信)

4,168件の閲覧回数
lpcxpresso_supp
NXP Employee
NXP Employee

So the msys issue will have nothing to do with hard fault error meesage you are seeing when you do a build.

That error is telling you that your project has two functions defined called "HardFault_Handler". The simplest way to solve this will be to delete one of them!

Regards,

MCUXpresso IDE Support

0 件の賞賛
返信

4,168件の閲覧回数
m_dietrich
Contributor I

Hi NXP-Team,

I did the suggested change with "msys-1.0-alternate.dll" alternative with no success.

I still get the same build error with the multiple definition of the `HardFault_Handler'.

Can you suggest anything else that might help me build the USB-KW41Z Sniffer into a Thread border router?

Thank you very much!

Kind regards,

Marlon

0 件の賞賛
返信

4,168件の閲覧回数
1901167646
Contributor II

hello 

maybe you can find someting useful in that build the example of ble_thread_router_wireless_uart by MCUXpresso but there were some errors  

Kind regards,

SJ YIN

0 件の賞賛
返信

4,168件の閲覧回数
lpcxpresso_supp
NXP Employee
NXP Employee

For details of how to resolve the "Couldn't reserve space for cygwin's heap" error see : 

Regards,

MCUXpresso IDE Support

0 件の賞賛
返信

4,168件の閲覧回数
1901167646
Contributor II

According to the method in the link, the build does not have an error, but the download is incorrect, prompting the missing file, restoring msys-1.0.dll, build or reporting an error.

there were debug errors

Program file does not exist
D:\MCUXpressio_IDE\workplace\usbkw41z_kw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos\Debug\usbkw41z_kw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos.axf not found
D:\MCUXpressio_IDE\workplace\usbkw41z_kw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos\Debug\usbkw41z_kw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos.axf not found
D:\MCUXpressio_IDE\workplace\usbkw41z_kw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos\Debug\usbkw41z_kw41z_wireless_examples_hybrid_ble_thread_router_wireless_uart_freertos.axf not found

4,168件の閲覧回数
m_dietrich
Contributor I

Hallo,

Trying to build the "thread end device example" I actually get a build error saying:

C:\...\kw41z_wireless_examples_thread_end_device_freertos\Debug/../nwk_ip/base/utils/debug_log.c:486: multiple definition of `HardFault_Handler'
./source/semihost_hardfault.o:C:\...\kw41z_wireless_examples_thread_end_device_freertos\Debug/../source/semihost_hardfault.c:72: first defined here
collect2.exe: error: ld returned 1 exit status
make: *** [kw41z_wireless_examples_thread_end_device_freertos.axf] Error 1

Thank you in advance for any help!

0 件の賞賛
返信

4,168件の閲覧回数
1901167646
Contributor II

hello 

maybe you can find someting useful in that build the example of ble_thread_router_wireless_uart by MCUXpresso but there were some errors  

Kind regards,

SJ YIN

0 件の賞賛
返信