doxygen support

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
4,267件の閲覧回数
billchadwick
Contributor III

Hi,

Is there any way to enable autodoc (for doxygen) in MCUXpresso

That is typing /**<cr> would produce e.g. a full function header template comment block

I have the eclox plugin installed but that is just the document generator.

On Eclipse CDT this is enabled with Window->Preferences->C/C++ ->Editor->"Documentation tool"

タグ(1)
0 件の賞賛
返信
1 解決策
4,263件の閲覧回数
ErichStyger
Specialist I

Do you have this enabled?

ErichS_0-1628498161839.png

This is the thing which works for me for years, see https://mcuoneclipse.com/2012/06/25/5-best-eclipse-plugins-1-eclox-with-doxygen-graphviz-and-mscgen/

I hope this helps,

Erich

 

元の投稿で解決策を見る

2 返答(返信)
4,264件の閲覧回数
ErichStyger
Specialist I

Do you have this enabled?

ErichS_0-1628498161839.png

This is the thing which works for me for years, see https://mcuoneclipse.com/2012/06/25/5-best-eclipse-plugins-1-eclox-with-doxygen-graphviz-and-mscgen/

I hope this helps,

Erich

 

4,260件の閲覧回数
billchadwick
Contributor III

That works. I missed it somehow.

Many thanks,

Bill

0 件の賞賛
返信