can't able to Receive the message from flex_CAN (CAN Communication)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

can't able to Receive the message from flex_CAN (CAN Communication)

1,274件の閲覧回数
tharun
Contributor I

Hello,
i have taken flex_can_interrupt_transfer example project to transmit(MIMXRT 1060) and receive data(MIMXRT 1020) using CAN communication .
we are transmitting message continuously from MIMXRT 1060 but only first message is received at MIMXRT 1020 and the interrupt is set for 1st message.
how can i receive all the message that are transmitted from MIMXRT1060.

(NOTE:Onboard CAN transceiver is used for both the MCU's )

could any one help me to resolve this problem.

thank you.

0 件の賞賛
返信
1 返信

1,220件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

I checked below message: 

NOTE:Onboard CAN transceiver is used for both the MCU's

If that means RT1060 & RT1020 shares the same CAN transceiver? If yes, that should cause the problem.

Mike

0 件の賞賛
返信