Using CMSIS-DSP with MCUXpresso SDK and IDE

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Using CMSIS-DSP with MCUXpresso SDK and IDE

ソリューションへジャンプ
4,185件の閲覧回数
gustavsl
Contributor III

I have downloaded MCUXpresso SDK 2.2 with CMSIS-DSP to develop for the MKL25Z128 on a custom board.

Using MCUXpresso IDE, I can't figure out how to use the bundled CMSIS-DSP. I tried following the instructions for adding CMSIS-DSP to KDS, but the CMSIS-DSP libraries fails to compile at some point.

Any tips?

Thanks.

ラベル(1)
1 解決策
3,831件の閲覧回数
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Gustavo,

Which error do you get while compiling? Please take a look to the following document for more information:

https://community.nxp.com/docs/DOC-335465 

Hope it helps!

Best Regards,
Carlos Mendoza
Technical Support Engineer

元の投稿で解決策を見る

2 返答(返信)
3,832件の閲覧回数
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Gustavo,

Which error do you get while compiling? Please take a look to the following document for more information:

https://community.nxp.com/docs/DOC-335465 

Hope it helps!

Best Regards,
Carlos Mendoza
Technical Support Engineer

3,831件の閲覧回数
gustavsl
Contributor III

Thank you for the guide! It's working now. :smileyhappy:

I guess I was messing up the include paths before.