Unresolved inclusion: <stdio.h>

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Unresolved inclusion: <stdio.h>

Jump to solution
35,136 Views
shauldorf
Contributor V

While importing project from MCUXpresso 10.3.1 to new IDE v. 11.0.0

I got question mark  ? Unresolved inclusion: <stdio.h>

MCUXpresso.png

1 Solution
34,404 Views
shauldorf
Contributor V

Hello Erich,

As usual you are in the right moment.

Thanks to you and Alexis .

Shaul

View solution in original post

6 Replies
34,406 Views
lpcxpresso_supp
NXP Employee
NXP Employee

Using the Tools->Fixup Parsers option on the Project Properties view's context sensitive menu (with the affect project selected) should resolve this issue for you.

[ This issue is described in the release info at: MCUXpresso IDE v11.0.0 Now Available ]

Regards,

MCUXpresso IDE Support

0 Kudos
Reply
34,403 Views
shauldorf
Contributor V

Thanks

Can you be more specific I can't fined

Tools->Fixup Parsers

In Project Properties view's.

Where this issue is described in release info exactly?

0 Kudos
Reply
34,403 Views
Alexis_A
NXP TechSupport
NXP TechSupport

Hi shauldorf‌,

You can find it here:

pastedImage_2.png

Best Regards,

Alexis Andalon

34,403 Views
shauldorf
Contributor V

Thanks

From yours screen I don't know to which menu his "Tools" belongs.

I'm not familiar with Eclipse perspective options and I'm using standard Menu Bar.

Sorry

Shaul

0 Kudos
Reply
34,401 Views
BlackNight
NXP Employee
NXP Employee

Hi Shaul,

it is in the context menu: select your project, then mouse right-click on it to get the menu.

I hope this helps,

Erich

0 Kudos
Reply
34,405 Views
shauldorf
Contributor V

Hello Erich,

As usual you are in the right moment.

Thanks to you and Alexis .

Shaul