USB middleware not showing up when creating new project

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

USB middleware not showing up when creating new project

跳至解决方案
2,528 次查看
jameso
Contributor II

I want to create a new project in MCUXpresso IDE v10.1.1 with USB middleware. However, USB is not an option under middleware even though USB is included in the SDK.
(See the attached images.)

标记 (2)
0 项奖励
回复
1 解答
2,345 次查看
lpcxpresso_supp
NXP Employee
NXP Employee

Unfortunately there are some restrictions with which components can be selected, as noted in section 5.1.1, "SDK New Project Wizard: Basic Project Creation and Settings", of the MCUXpresso IDE v10.1 User Guide:

Note: Some middleware components such as USB, are not currently compatible with the New project wizard functionality and so will be hidden. The recommended approach if such components are required is to import an example including the component and then modify this as required. Please see SDK Project Component Management [53] for details of how this might be done.

Regards,

MCUXpresso IDE Support

在原帖中查看解决方案

0 项奖励
回复
1 回复
2,346 次查看
lpcxpresso_supp
NXP Employee
NXP Employee

Unfortunately there are some restrictions with which components can be selected, as noted in section 5.1.1, "SDK New Project Wizard: Basic Project Creation and Settings", of the MCUXpresso IDE v10.1 User Guide:

Note: Some middleware components such as USB, are not currently compatible with the New project wizard functionality and so will be hidden. The recommended approach if such components are required is to import an example including the component and then modify this as required. Please see SDK Project Component Management [53] for details of how this might be done.

Regards,

MCUXpresso IDE Support

0 项奖励
回复