USB middleware not showing up when creating new project

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB middleware not showing up when creating new project

Jump to solution
2,526 Views
jameso
Contributor II

I want to create a new project in MCUXpresso IDE v10.1.1 with USB middleware. However, USB is not an option under middleware even though USB is included in the SDK.
(See the attached images.)

Tags (2)
0 Kudos
Reply
1 Solution
2,343 Views
lpcxpresso_supp
NXP Employee
NXP Employee

Unfortunately there are some restrictions with which components can be selected, as noted in section 5.1.1, "SDK New Project Wizard: Basic Project Creation and Settings", of the MCUXpresso IDE v10.1 User Guide:

Note: Some middleware components such as USB, are not currently compatible with the New project wizard functionality and so will be hidden. The recommended approach if such components are required is to import an example including the component and then modify this as required. Please see SDK Project Component Management [53] for details of how this might be done.

Regards,

MCUXpresso IDE Support

View solution in original post

0 Kudos
Reply
1 Reply
2,344 Views
lpcxpresso_supp
NXP Employee
NXP Employee

Unfortunately there are some restrictions with which components can be selected, as noted in section 5.1.1, "SDK New Project Wizard: Basic Project Creation and Settings", of the MCUXpresso IDE v10.1 User Guide:

Note: Some middleware components such as USB, are not currently compatible with the New project wizard functionality and so will be hidden. The recommended approach if such components are required is to import an example including the component and then modify this as required. Please see SDK Project Component Management [53] for details of how this might be done.

Regards,

MCUXpresso IDE Support

0 Kudos
Reply