Target reported errors

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Target reported errors

3,513件の閲覧回数
Prudhvi_Raj
Contributor I

Tried to debug sdk by MCUXpresso IDE ,occuring a error such as target reported errors .provide solution as soon as possible.

Refer to the attachment.

0 件の賞賛
返信
4 返答(返信)

3,484件の閲覧回数
Prudhvi_Raj
Contributor I

Hi @Harry_Zhang 

The board is powered by debug port and tried to debug, still i am getting the same error same as earlier.

0 件の賞賛
返信

3,471件の閲覧回数
Harry_Zhang
NXP Employee
NXP Employee

Hi @Prudhvi_Raj 

On another board, i reproduced this issue.

HangZhang_1-1718272093484.pngHangZhang_1-1718272093484.png

When i changed to jlink.

It can work.

HangZhang_2-1718272156104.pngHangZhang_2-1718272156104.png

Hope this will help you.

BR

Hang

0 件の賞賛
返信

3,474件の閲覧回数
Harry_Zhang
NXP Employee
NXP Employee

Hi @Prudhvi_Raj 

I tested my board, 

HangZhang_0-1718266886254.pngHangZhang_0-1718266886254.png

HangZhang_1-1718266954292.pngHangZhang_1-1718266954292.png

It can work.

I watched your error message,

It reported that the wire not connected,

So can you change another wire?

BR

Hang

 

0 件の賞賛
返信

3,495件の閲覧回数
Harry_Zhang
NXP Employee
NXP Employee

Hi @Prudhvi_Raj 

According to the picture, this error is due to not connecting to the core.

So please check if this board is powered on and if it is connected to the debug port.

Hope this will help you.

BR

Hang

0 件の賞賛
返信