Refresh SDK Repository Issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Refresh SDK Repository Issue

ソリューションへジャンプ
5,722件の閲覧回数
oliviermonnom
Contributor II

Hi, 

I'm on Ubuntu 18.04 and since 2 days I've an issue when I open MCUXpresso IDE.

Once opened, the IDE (11.2.1) is doing a "Refresh SDK Repository..." and it takes full processing time (I see this with htop) until it crashes (internal error, see photo). I've downgraded to 11.1.1 (removing also all the config files from my home folder) and I have the same result.

I can't use anymore the IDE for my work! I can't figure out what is happening here.

My java version:

$ java -version
openjdk version "11.0.8" 2020-07-14
OpenJDK Runtime Environment (build 11.0.8+10-post-Ubuntu-0ubuntu118.04.1)
OpenJDK 64-Bit Server VM (build 11.0.8+10-post-Ubuntu-0ubuntu118.04.1, mixed mode, sharing)

Any help or advice welcome,

Thank you,

Olivier

0 件の賞賛
返信
1 解決策
5,702件の閲覧回数
oliviermonnom
Contributor II

Hi,

I did a new workspace in a new fresh folder but inside a git versioning folder -> same problem.

Then I did a new workspace in a new fresh folder outside this folder -> it worked.

Problem solved, thank you.

Olivier

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
5,715件の閲覧回数
converse
Senior Contributor V

Suggest you post the log file:

<workspace>/.metadata/.log

Also, try starting MCUXpresso with a new, empty workspace.

0 件の賞賛
返信
5,703件の閲覧回数
oliviermonnom
Contributor II

Hi,

I did a new workspace in a new fresh folder but inside a git versioning folder -> same problem.

Then I did a new workspace in a new fresh folder outside this folder -> it worked.

Problem solved, thank you.

Olivier

0 件の賞賛
返信